Hi, open source compiling and flashing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, open source compiling and flashing

1,652 Views
danielf_garcia
Contributor I

Hi, I am new at Freescale, I used to worked with T.I. but it's dificult to find open source tools for my projects,  so I would like to know if here is the place where I can find tools for Liux (Ubuntu) open source for embedded systems where I can compile and flash in easy ways, not with just close-source programas and comunication protocols.

I am developing a proyect that needs a microcontroller and a digital signal controller, so Can anybody suggest me some integrated circuits that I can use, and the tools for development (I always use C for programming by the way)?

Thanks,

Daniel

0 Kudos
Reply
2 Replies

1,536 Views
pgo
Senior Contributor V

Hi Daniel,

USBDM supports using Eclipse+ARM-GCC on linux (tested on ubuntu).

See this page for downloads:

USBDM - Browse /Version 4.10.6/Software at SourceForge.net

Introduction at:

USBDM: USBDM Debugger interface for Freescale RS08,HCS08,HCS12,Coldfire and ARM-Kinetis Devices.

Some information on Eclipse setup is available on:

USBDM: Eclipse - Install (Codesourcery, GNU tools)

bye

0 Kudos
Reply

1,536 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

CW10.5 doesn't support linux platform.

you can get access to the ARM GCC Linux build tools via the ARM Launch pad:

https://launchpad.net/gcc-arm-embedded

See:

http://mcuoneclipse.com/2013/07/20/dyi-free-toolchain-for-kinetis-part-1-gnu-arm-build-tools/

0 Kudos
Reply