[KL26Z] Differential ADC with bad readings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[KL26Z] Differential ADC with bad readings

Jump to solution
1,847 Views
karennisley
Contributor I


I am attempting to configure the ADC on the FRDM-KL26Z in differential mode such that it takes a reading every time the read function is called in main().

I have an init() function:

void adc_init(void)

{

    OSC0_CR |= OSC_CR_ERCLKEN(0x1);         //enable oscerclk

    SIM->SCGC5 |= SIM_SCGC5_PORTE_MASK;     //enable clock for PORT

    SIM_>SCGC6 |= SIM_SCGC6_ADC0_MASK;      //enable the clock to ADC

    PORTE->PCR[20] |= PORT_PCR_MUX(0U);       //pin alt functions

    PORTE->PCR[21] |= PORT_PCR_MUX(0U);

    //Configure CFG1 & 2

    ADC0_CFG1 = ADC_CFG1_MODE(0x3);             //resolution 16 bit differential

                 //| ADC_CFG1_ADIV(0x2));         //& clock/2

    adc_cal();                              //call calibration as specified in datasheet flowchart

    //SC2- nothing here

    //SC3- nothing here

    ADC0_SC1A = (ADC_SC1_DIFF(0x1) | ADC_SC1_ADCH(0x0));       //enable differential mode & select input channel

    //ADC0_SC1B = (ADC_SC1_DIFF(0x1) | ADC_SC1_ADCH(0x3));       //enable differential mode & select input channel

    //software trigger & Vrefh and Vrefl are default

}

and a calibration function that is called by the adc_init();

void adc_cal(void)

{   //"for best calibration results" section is being ignored!!

    //ADC0_SC2 = ADC_SC2_ADTRG(0x0);          //clear ADTRG bit

    ADC0_SC3 = ADC_SC3_CAL_MASK;            //'user sets sc3[cal] and itll automatically begin'

    /* Wait until calibration is finished */

    while(ADC0->SC3 & ADC_SC3_CAL_MASK);

    //calibrate high side

    uint16_t cal_var_h = 0;                     //make a 16 bit var

    cal_var_h = (ADC0_CLP0 & ~ADC_CLP0_CLP0_MASK) + (ADC0_CLP1 & ~ADC_CLP1_CLP1_MASK) + (ADC0_CLP2 & ~ADC_CLP2_CLP2_MASK)+ (ADC0_CLP3 & ~ADC_CLP3_CLP3_MASK) + (ADC0_CLP4 & ~ADC_CLP4_CLP4_MASK) + (ADC0_CLPS & ~ADC_CLPS_CLPS_MASK);           //sum all the calibrations

    cal_var_h = cal_var_h / 2;              //divide the variable by two

    cal_var_h = cal_var_h & 0x800;          //set the msb

    ADC0_PG = cal_var_h;                    //store it where it belongs

    //calibrate low side

    uint16_t cal_var_l = 0;                     //make a 16 bit var

    cal_var_l = (ADC0_CLM0 & ~ADC_CLM0_CLM0_MASK) + (ADC0_CLM1 & ~ADC_CLM1_CLM1_MASK) + (ADC0_CLM2 & ~ADC_CLM2_CLM2_MASK)+ (ADC0_CLM3 & ~ADC_CLM3_CLM3_MASK) + (ADC0_CLM4 & ~ADC_CLM4_CLM4_MASK) + (ADC0_CLMS & ~ADC_CLMS_CLMS_MASK);           //sum all the calibrations

    cal_var_l = cal_var_l / 2;              //divide the variable by two

    cal_var_l = cal_var_l & 0x800;          //set the msb

    ADC0_MG = cal_var_l;                    //store it where it belongs

    //ADC0_SC3 = ADC_SC3_CAL(0x0);            //disable calibration

    if(ADC0_SC3 != 0)                       //check for success

    {

        uart_putc('f');                     //complain on the uart if calibration failed

    }

}

and a read function

int16_t adc_get_read(uint8_t channel)    //signed int should handle the 2's compliment

{

    if(channel == 0)

    {

        //ADC0_CFG2 = ADC_CFG2_MUXSEL(0x0);

        ADC0_SC1A |= ADC_SC1_ADCH(0x0);    //trigger conversion on ch0

        while((ADC0_SC1A & ADC_SC1_COCO_MASK) == 0)  //conversion complete flag

        {

            //wait for the conversion to complete

        }

        //ADC0_SC1A = ADC_SC1_COCO(0x0);      //Reset COCO use the shift in

        return ADC0_RA;                     //result register, should clear COCO

    }

/*nonfunctional channel 1 code snipped for brevity*/

    else    //in case of burp

    {

        uart_putc('f');                     //complain on the uart if fail

        return 0;

    }

}

The function calls in main() look like

reading0 = adc_get_read(0);

uart_outHex(reading0);          //sends the reading over the UART to terminal in ascii encoded hex

The frdm board is setup with R9 jumpered to enable external Vrefh, and Vrefh tied to 3.3V. DP0 is set to the output of the DAC and DM0 is set to ground.
The DAC, UART, and uart_outHex have been confirmed to work as expected and designed.

The failure is that the ADC reads very low values (0 through about 3, in hex) and very high values (0xFFFFFFFC through 0xFFFFFFFF) with no middle ground, and typically sticks to either high or low values with random deviations to the other value. I suspect that it is a clocking issue, but I can not determine where. Can anyone advise me? Thank you.

0 Kudos
Reply
1 Solution
1,310 Views
karennisley
Contributor I

cal_var_h and cal_var_l are calculated incorrectly- should just be a sum, and 0x800 should be 0x8000.

View solution in original post

0 Kudos
Reply
2 Replies
1,311 Views
karennisley
Contributor I

cal_var_h and cal_var_l are calculated incorrectly- should just be a sum, and 0x800 should be 0x8000.

0 Kudos
Reply
1,309 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Karen,

You can refer the ADC16_DoAutoCalibration function in KSDK2.0 for KL26.

ADC16_DoAutoCalibration.png

I recommand you use the examples in KSDK2.0. (If you have not used it, please read Introducing Kinetis SDK v2 first.)

driver_examples in SDK_2.0_FRDM-KL26Z.png

You can download and install it refer the methods in How to: install KSDK 2.0.

Best Regards,

Robin

0 Kudos
Reply