KL25 RTC Power

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL25 RTC Power

1,927 次查看
engdigital
Contributor I

Hello,

from what I understand, KL25 series has no battery pin and the RTC shares its power domain with the Core. I've read in another question that it is possible to put the KL25 in a low power state when the main power supply goes off.

Do I have to implement this on my own e.g. w/ an interrupt on a IO/Comparator pin or is there something already integrated?

Is there any code sample on the matter?


Thanks.

标记 (3)
0 项奖励
回复
2 回复数

1,783 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

KL25 has various low power mode, while it also need main power(power to KL25's VDD pin). Customer could low down the main power to 1.71V, if main power was taken off, the KL25 was off too.

About KL25 low power mode example code, customer could download KL25 example code(bare-metal) from here.

NXP also provides KSDK software for KL25 product, please download software from here.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,783 次查看
mjbcswitzerland
Specialist V
0 项奖励
回复