KL16 Erase Flash Sector execution time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL16 Erase Flash Sector execution time

跳至解决方案
1,607 次查看
seanwu
Contributor IV

Dear sir,

In datasheet, Erase Flash Sector execution time is from 14~114ms

What are the conditions that affect Erase Time?

seanwu_0-1708332664105.png

 

Thanks.

BR,

Sean Wu

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,574 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport
Hi, Sean,
This is AE team reply for large erasing time tolerance:
"
There is a footnote to describe the max. value: Maximum time based on expectations at cycling end-of-life. I think the erase time is affected by the physical characteristics of flash.  These factors may affect the flash physical characteristics, such as production process deviation, the number of sectors/blocks erased, the length of flash operating time
"
Hope it can help you
BR
XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,575 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport
Hi, Sean,
This is AE team reply for large erasing time tolerance:
"
There is a footnote to describe the max. value: Maximum time based on expectations at cycling end-of-life. I think the erase time is affected by the physical characteristics of flash.  These factors may affect the flash physical characteristics, such as production process deviation, the number of sectors/blocks erased, the length of flash operating time
"
Hope it can help you
BR
XiangJun Rong
0 项奖励
回复
1,528 次查看
seanwu
Contributor IV
Dear sir,

Thanks for your help.
0 项奖励
回复
1,585 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked the AE team of Kinetis for the question why the erasing time tolerance is so large for KL family.

I will update the ticket after I get reply.

BR

XiangJun Rong

0 项奖励
回复