KL16 Erase Flash Sector execution time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL16 Erase Flash Sector execution time

Jump to solution
2,486 Views
seanwu
Contributor IV

Dear sir,

In datasheet, Erase Flash Sector execution time is from 14~114ms

What are the conditions that affect Erase Time?

seanwu_0-1708332664105.png

 

Thanks.

BR,

Sean Wu

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,453 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport
Hi, Sean,
This is AE team reply for large erasing time tolerance:
"
There is a footnote to describe the max. value: Maximum time based on expectations at cycling end-of-life. I think the erase time is affected by the physical characteristics of flash.  These factors may affect the flash physical characteristics, such as production process deviation, the number of sectors/blocks erased, the length of flash operating time
"
Hope it can help you
BR
XiangJun Rong

View solution in original post

0 Kudos
Reply
3 Replies
2,454 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport
Hi, Sean,
This is AE team reply for large erasing time tolerance:
"
There is a footnote to describe the max. value: Maximum time based on expectations at cycling end-of-life. I think the erase time is affected by the physical characteristics of flash.  These factors may affect the flash physical characteristics, such as production process deviation, the number of sectors/blocks erased, the length of flash operating time
"
Hope it can help you
BR
XiangJun Rong
0 Kudos
Reply
2,407 Views
seanwu
Contributor IV
Dear sir,

Thanks for your help.
0 Kudos
Reply
2,464 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked the AE team of Kinetis for the question why the erasing time tolerance is so large for KL family.

I will update the ticket after I get reply.

BR

XiangJun Rong

0 Kudos
Reply