KEA128 + BLE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,079件の閲覧回数
irmantasbudrys
Contributor III

Hello,

 

I am using FRDM DEV BRD KEAZ128 and S32. I have downloaded FRDM-KEA-QSP.zip package in which I found Lab9_BLE_KEA128. I would like to use BLE in my project. Where can I found more info how to start and use this example? Which BLE board this lab example is using?

Thank you.

 

Best Regards,

IB

1 解決策
1,956件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Irmantas Budrys,

     The relate info for KEA128 can be found in these ways:

1. FRDM-KEA Lab Examples and Board Overview.pdf in the QSP package

Folder: FRDM-KEA-QSP\Quick Start Package v5\SDK Drivers and Code Example Projects

2. Please refer to the ftf document:

http://cache.nxp.com/files/FTF_2015/ftf-acc-F1112.pdf?fsrch=1&sr=2&pageNum=1 

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,957件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Irmantas Budrys,

     The relate info for KEA128 can be found in these ways:

1. FRDM-KEA Lab Examples and Board Overview.pdf in the QSP package

Folder: FRDM-KEA-QSP\Quick Start Package v5\SDK Drivers and Code Example Projects

2. Please refer to the ftf document:

http://cache.nxp.com/files/FTF_2015/ftf-acc-F1112.pdf?fsrch=1&sr=2&pageNum=1 

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------