KE06 KBI question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE06 KBI question

1,502 Views
davidsherman
Senior Contributor I

Looking into the KE06 reference manual, I noticed something I hadn't before.  On page 698, it says "The KBI module allows up to eight pins to act as additional interrupt sources."  Does this mean only 8 pins can be enabled at a time?  That seems strange if there are 32 pins available to the KBI.

0 Kudos
Reply
3 Replies

1,360 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi David,

    Just as Mark have said, it is the KE06 reference manual error, KE06 each KBI module have 32 pin, so the KBI module allows up to 32 pins to act as additional interrupts sources.

  From the interrupt vector assignments, we also can find it.

54.jpg

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,360 Views
davidsherman
Senior Contributor I

Thanks, I just wanted to make sure it was a typo and not a limitation that only 8 of the 32 pins can be enabled at a time.

0 Kudos
Reply

1,360 Views
mjbcswitzerland
Specialist V

Hi

I haven't noticed any restrictions so it is probably a cut-and-paste error in the manual since the text is shared with the KE02, which has an 8 bit KBI controller.

Regards

Mark