KE06 KBI question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KE06 KBI question

1,511 次查看
davidsherman
Senior Contributor I

Looking into the KE06 reference manual, I noticed something I hadn't before.  On page 698, it says "The KBI module allows up to eight pins to act as additional interrupt sources."  Does this mean only 8 pins can be enabled at a time?  That seems strange if there are 32 pins available to the KBI.

0 项奖励
回复
3 回复数

1,369 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi David,

    Just as Mark have said, it is the KE06 reference manual error, KE06 each KBI module have 32 pin, so the KBI module allows up to 32 pins to act as additional interrupts sources.

  From the interrupt vector assignments, we also can find it.

54.jpg

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,369 次查看
davidsherman
Senior Contributor I

Thanks, I just wanted to make sure it was a typo and not a limitation that only 8 of the 32 pins can be enabled at a time.

0 项奖励
回复

1,369 次查看
mjbcswitzerland
Specialist V

Hi

I haven't noticed any restrictions so it is probably a cut-and-paste error in the manual since the text is shared with the KE02, which has an 8 bit KBI controller.

Regards

Mark