KDS debug with USBDM issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KDS debug with USBDM issue

2,980件の閲覧回数
JiaAn
Contributor I

Hi guys,

I am trying to debug with USBDM on KDS. I am running on Windows 7 x32 / KDSv3.2.0 / USBDM4_12_1_240 . And when I press debug as USBDM C++ session it shows me this error message.

JiaAn_0-1628133494429.png

 

I already tried C:\Program Files\pgo\USBDM 4.12.1.240\UsbdmFlashProgrammer.exe and it can erase and program Flash without any error message. This problem only happening in KDS debug. Can anyone help? Thanks.

 

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,904件の閲覧回数
pgo
Senior Contributor V

Hi,

A bit of a late reply  - Check the communication speed being used.

What is the target device?

bye

0 件の賞賛
返信

2,968件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Would be possible that you use MCUXpresso?

 

We do not recommend using the KSD

 

Regards

 

0 件の賞賛
返信

2,963件の閲覧回数
JiaAn
Contributor I

But can USBDM working on MCUxpresso?

How to build a project for MKL17Z256VLH4 and debug with USBDM on MCUxpresso?

0 件の賞賛
返信

2,945件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

No, sorry no

0 件の賞賛
返信