KDS debug with USBDM issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS debug with USBDM issue

2,935 Views
JiaAn
Contributor I

Hi guys,

I am trying to debug with USBDM on KDS. I am running on Windows 7 x32 / KDSv3.2.0 / USBDM4_12_1_240 . And when I press debug as USBDM C++ session it shows me this error message.

JiaAn_0-1628133494429.pngJiaAn_0-1628133494429.png

 

I already tried C:\Program Files\pgo\USBDM 4.12.1.240\UsbdmFlashProgrammer.exe and it can erase and program Flash without any error message. This problem only happening in KDS debug. Can anyone help? Thanks.

 

Labels (2)
0 Kudos
Reply
4 Replies

2,859 Views
pgo
Senior Contributor V

Hi,

A bit of a late reply  - Check the communication speed being used.

What is the target device?

bye

0 Kudos
Reply

2,923 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Would be possible that you use MCUXpresso?

 

We do not recommend using the KSD

 

Regards

 

0 Kudos
Reply

2,918 Views
JiaAn
Contributor I

But can USBDM working on MCUxpresso?

How to build a project for MKL17Z256VLH4 and debug with USBDM on MCUxpresso?

0 Kudos
Reply

2,900 Views
vicentegomez
NXP TechSupport
NXP TechSupport

No, sorry no

0 Kudos
Reply