K70 Graphical LCD controller support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K70 Graphical LCD controller support

跳至解决方案
2,660 次查看
danif
Contributor I

It is mentioned in the specification of K70 controller that it has Graphical LCD controller for 800x600 pixel resolution LCD. I have three questions.

1 - How to run a graphical LCD with more than 800x600 resolution.

2 - Can K70 enter into low power modes while Graphical LCD keeps on displaying without any disturbance.

3 - Can a graphical LCD controller be used to run a segmented LCD..if yes how?

Thanks,

Dani

标签 (1)
0 项奖励
回复
1 解答
2,382 次查看
apanecatl
Senior Contributor II

1.- You can interface the LCDC module with larger displays however the controller will only send a 800x600 image, leaving the rest of the display inactive.

2.- As you can see in the following table extracted from the Reference manual, the LCDC module retains full functionality in VLPR and VLPW

4012_4012.png

3.- I'm afraid the K70 LCDC module can only interface with graphic displays, however you can use any of the GPIO ports to achieve segment LCD communication.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,383 次查看
apanecatl
Senior Contributor II

1.- You can interface the LCDC module with larger displays however the controller will only send a 800x600 image, leaving the rest of the display inactive.

2.- As you can see in the following table extracted from the Reference manual, the LCDC module retains full functionality in VLPR and VLPW

4012_4012.png

3.- I'm afraid the K70 LCDC module can only interface with graphic displays, however you can use any of the GPIO ports to achieve segment LCD communication.

0 项奖励
回复
2,382 次查看
danif
Contributor I

Thanks Pedro,

Thanks for the reply. This is really helpful.

Regards,

Dani

0 项奖励
回复