K70 Graphical LCD controller support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 Graphical LCD controller support

ソリューションへジャンプ
2,651件の閲覧回数
danif
Contributor I

It is mentioned in the specification of K70 controller that it has Graphical LCD controller for 800x600 pixel resolution LCD. I have three questions.

1 - How to run a graphical LCD with more than 800x600 resolution.

2 - Can K70 enter into low power modes while Graphical LCD keeps on displaying without any disturbance.

3 - Can a graphical LCD controller be used to run a segmented LCD..if yes how?

Thanks,

Dani

ラベル(1)
0 件の賞賛
返信
1 解決策
2,373件の閲覧回数
apanecatl
Senior Contributor II

1.- You can interface the LCDC module with larger displays however the controller will only send a 800x600 image, leaving the rest of the display inactive.

2.- As you can see in the following table extracted from the Reference manual, the LCDC module retains full functionality in VLPR and VLPW

4012_4012.png

3.- I'm afraid the K70 LCDC module can only interface with graphic displays, however you can use any of the GPIO ports to achieve segment LCD communication.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,374件の閲覧回数
apanecatl
Senior Contributor II

1.- You can interface the LCDC module with larger displays however the controller will only send a 800x600 image, leaving the rest of the display inactive.

2.- As you can see in the following table extracted from the Reference manual, the LCDC module retains full functionality in VLPR and VLPW

4012_4012.png

3.- I'm afraid the K70 LCDC module can only interface with graphic displays, however you can use any of the GPIO ports to achieve segment LCD communication.

0 件の賞賛
返信
2,373件の閲覧回数
danif
Contributor I

Thanks Pedro,

Thanks for the reply. This is really helpful.

Regards,

Dani

0 件の賞賛
返信