K70 ADC hardware average function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K70 ADC hardware average function

跳至解决方案
3,141 次查看
hemanthkumarven
Contributor II

All,

In the K70 Reference Manual, under section 39, 16-bit ADC it has been mentioned that hardware average function is supported.

In the K70 Datasheet document, (Doc. Name: K70P256M120SF3) under table -29 it is mentioned that no ADC hardware averaging function.

Is the hardware averaging function present as part of 16-bit ADC?

Thanks

Hemanth

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
2,568 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,569 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,568 次查看
hemanthkumarven
Contributor II

Thanks for the Quick Reply Jorge..

Really appreciated..

Hemanth

0 项奖励
回复