K70 ADC hardware average function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K70 ADC hardware average function

ソリューションへジャンプ
3,136件の閲覧回数
hemanthkumarven
Contributor II

All,

In the K70 Reference Manual, under section 39, 16-bit ADC it has been mentioned that hardware average function is supported.

In the K70 Datasheet document, (Doc. Name: K70P256M120SF3) under table -29 it is mentioned that no ADC hardware averaging function.

Is the hardware averaging function present as part of 16-bit ADC?

Thanks

Hemanth

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,563件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,564件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

Yes, hardware averaging is supported by ADC in K70. I think you refer to the next part of the datasheet right?

ADC.png

The "No ADC hardware averaging" just represents a condition. It means that a Crate between 37.037 and 461.467 Ksps can be achieved using continuous conversions and *without* enabling hardware averaging, but it does not mean that averaging is not supported.

I hope this clarifies.

Regards!,

Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,563件の閲覧回数
hemanthkumarven
Contributor II

Thanks for the Quick Reply Jorge..

Really appreciated..

Hemanth

0 件の賞賛
返信