K66 : Legacy receive buffer descriptor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K66 : Legacy receive buffer descriptor

ソリューションへジャンプ
1,989件の閲覧回数
koichisakagami
Contributor II

Dear community,
We are checking a Legacy receive buffer descriptor.

In the manual K66P144M180SF5RMV2 Rev. 2, Table 50-33. Receive buffer descriptor field definitions
it is described that the Field "L" indicates the  "Last in frame".
       0 : The buffer is not the last in a frame.
       1 : The buffer is the last in a frame.

[Question]
       How do I recognize the first in a frame ?

Best Regards,
  Koichi Sakagami

ラベル(1)
0 件の賞賛
返信
1 解決策
1,868件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,869件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 件の賞賛
返信