K66 : Legacy receive buffer descriptor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66 : Legacy receive buffer descriptor

Jump to solution
1,941 Views
koichisakagami
Contributor II

Dear community,
We are checking a Legacy receive buffer descriptor.

In the manual K66P144M180SF5RMV2 Rev. 2, Table 50-33. Receive buffer descriptor field definitions
it is described that the Field "L" indicates the  "Last in frame".
       0 : The buffer is not the last in a frame.
       1 : The buffer is the last in a frame.

[Question]
       How do I recognize the first in a frame ?

Best Regards,
  Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
1,820 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

View solution in original post

0 Kudos
Reply
1 Reply
1,821 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Koichi,

I think the L flag is a IPv4 specific flag, the "Flags/Fragment offset" data in IP layer can determine the L bit in RxBD.

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply