K60 ADC eternal sequencing of 12 inputs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 ADC eternal sequencing of 12 inputs

ソリューションへジャンプ
1,690件の閲覧回数
michelc
Contributor I

Hi, I have to scan 12 single ended inputs of ADC1 with 8 bits result eternally.

I would like to do this without CPU intervention, so in DMA mode modulo 24, using 2 buffers of 12 bytes.

Is this possible? (cfr. X-Scale Stellaris can)

Thx,

Michel

ラベル(1)
0 件の賞賛
返信
1 解決策
1,386件の閲覧回数
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,387件の閲覧回数
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

0 件の賞賛
返信
1,386件の閲覧回数
michelc
Contributor I

Thanks Norm, that's just what I was looking for!

Michel

0 件の賞賛
返信