K60 ADC eternal sequencing of 12 inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 ADC eternal sequencing of 12 inputs

跳至解决方案
1,786 次查看
michelc
Contributor I

Hi, I have to scan 12 single ended inputs of ADC1 with 8 bits result eternally.

I would like to do this without CPU intervention, so in DMA mode modulo 24, using 2 buffers of 12 bytes.

Is this possible? (cfr. X-Scale Stellaris can)

Thx,

Michel

标签 (1)
0 项奖励
回复
1 解答
1,482 次查看
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,483 次查看
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

0 项奖励
回复
1,482 次查看
michelc
Contributor I

Thanks Norm, that's just what I was looking for!

Michel

0 项奖励
回复