K10D input protection diode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10D input protection diode

2,932件の閲覧回数
ScottKerstein
Contributor III

The PTC1 pin on the K10D is configured for input capture function, but it also has an alternate analog function which is not used in the design.

Is the input protection to VDD through a clamping diode still available when configured for input capture, or just when the pin is configured as an analog function?

What kind of internal protection is offered on the default Port IO pins?

Thanks in advance.

Scott

ラベル(2)
6 返答(返信)

2,741件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Scott,

The ESD protection circuit (clamping diode) is applied for each port IO pin, whatever it configured for input capture or analog function.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,741件の閲覧回数
ScottKerstein
Contributor III

Thanks.  It appears the other I/O isn't protect.  Why?

0 件の賞賛
返信

2,741件の閲覧回数
egoodii
Senior Contributor III

There is no diode to VDD on all GPIO-capable pins to allow 5V input signal level tolerance, irrespective of actual Vdd voltage.

0 件の賞賛
返信

2,741件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

For the 5V tolerant I/O with special design, the diode not connect to VDD, while instead to a ESD Bus.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,741件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

I am not sure "the other I/O" means?

Best regards,

Ma Hui

0 件の賞賛
返信

2,741件の閲覧回数
egoodii
Senior Contributor III

Any pin that CAN be GPIO physically does NOT have said diode to VDD, and can accept -0.3 to 5.5V at any time, in any mode.  The protection elements do not change based on 'pin mode'