K10D input protection diode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K10D input protection diode

1,897 次查看
ScottKerstein
Contributor III

The PTC1 pin on the K10D is configured for input capture function, but it also has an alternate analog function which is not used in the design.

Is the input protection to VDD through a clamping diode still available when configured for input capture, or just when the pin is configured as an analog function?

What kind of internal protection is offered on the default Port IO pins?

Thanks in advance.

Scott

6 回复数

1,706 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Scott,

The ESD protection circuit (clamping diode) is applied for each port IO pin, whatever it configured for input capture or analog function.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,706 次查看
ScottKerstein
Contributor III

Thanks.  It appears the other I/O isn't protect.  Why?

0 项奖励
回复

1,706 次查看
egoodii
Senior Contributor III

There is no diode to VDD on all GPIO-capable pins to allow 5V input signal level tolerance, irrespective of actual Vdd voltage.

0 项奖励
回复

1,706 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

For the 5V tolerant I/O with special design, the diode not connect to VDD, while instead to a ESD Bus.


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,706 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

I am not sure "the other I/O" means?

Best regards,

Ma Hui

0 项奖励
回复

1,706 次查看
egoodii
Senior Contributor III

Any pin that CAN be GPIO physically does NOT have said diode to VDD, and can accept -0.3 to 5.5V at any time, in any mode.  The protection elements do not change based on 'pin mode'