K10 using I2S MIC.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 using I2S MIC.

1,611件の閲覧回数
c393
Contributor II

I have a K10P144M120 design. I have a I2S MIC connected to I2S1_RXD0, I2S1_BCLK and I2S1_RX_FS. Can I configure the SAI module for receive only? Do I have to configure the transmit?  It appears that the RX BCLK source is from the transmit BCLK. Can I configure the transmit but do not configure the I/O pins? 

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

1,446件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Dennis

Yes, you can configure it as receiver only. For your last question, I cannot understand it clearly. Would you please to make me clear? Thanks.

Best Regards

Paul

0 件の賞賛
返信