Copy flash from one chip to another using JTAG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Copy flash from one chip to another using JTAG

跳至解决方案
2,234 次查看
marlonsmith
Contributor IV

Hi everyone,

I've written some code for the K20 chip, and I'm wondering if it's safe to use a JTAG programmer to copy that code from one chip to another.  Is there anything in memory that's perhaps read-only or reserved that could cause problems when dumping the entire memory from one K20 to another?

Thanks

Marlon

标记 (2)
0 项奖励
回复
1 解答
2,040 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

This really depends the JTAG programmer. As normal, if programmer support this function, it should be safe.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,041 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

This really depends the JTAG programmer. As normal, if programmer support this function, it should be safe.

Best Regards

Paul

0 项奖励
回复