K10 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10 series

2,313 Views
mahdishojaei039
Contributor II

H,

i have MK10FN1M0VLQ12 .

is it possible use Ulink Programmer ? or any thing else universal programmer ?

thanks.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,247 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello mahdi shojaei

 

Yes, it is possible to use the ULINK debugger with the kinetis k10 since the MCUXpresso IDE supports this tool.

pastedImage_3.png

 

 Also, you can check our recommended debuggers at the tab "Tools&Software" on this page Arm Cortex-M4|Kinetis K10 120 MHz 32-bit MCUs | NXP. These suggestions can be the P&E Universal Multilink or the LPC-Link2.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

2,247 Views
mahdishojaei039
Contributor II

Thank you Omar Anguiano .

0 Kudos
Reply