K10 series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 series

2,199件の閲覧回数
mahdishojaei039
Contributor II

H,

i have MK10FN1M0VLQ12 .

is it possible use Ulink Programmer ? or any thing else universal programmer ?

thanks.

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,133件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello mahdi shojaei

 

Yes, it is possible to use the ULINK debugger with the kinetis k10 since the MCUXpresso IDE supports this tool.

pastedImage_3.png

 

 Also, you can check our recommended debuggers at the tab "Tools&Software" on this page Arm Cortex-M4|Kinetis K10 120 MHz 32-bit MCUs | NXP. These suggestions can be the P&E Universal Multilink or the LPC-Link2.

 

Let me know if this is helpful, if you have more questions do not hesitate to ask me.

Best regards,

Omar

2,133件の閲覧回数
mahdishojaei039
Contributor II

Thank you Omar Anguiano .

0 件の賞賛
返信