Hello David,
(1) On KDS, when you create project for your board , you can select the chip of SKEAZ128xxxx4,
this is the chip of your board . And yes, the ksdk doesn't support this chip, while , you can select
the Processor Expert(PE) when you create project , also can create bare board project (without PE).

(2) About the UART baud rate , i don't know what the value of other register about it , so you can refer to
the formula to calculate :

or if you create one PE project , you can directly configure the baud rate on the UART
component view:

Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------