Interfacing DS1307 with KL46

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing DS1307 with KL46

1,897件の閲覧回数
abulhasan_cas
Contributor I

Hi all,

     Good day to you.

     I'm using KL46 processor and we are in need to interface an external RTC chip DS1307 with KL46. Can anyone suggest me how to get the output of DS1307 and feed it to the KL46 in I2C.

Abul Hasan

0 件の賞賛
返信
2 返答(返信)

1,688件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have created an open source Processor Expert component which supports both the DS3232 and DS1307:

http://mcuoneclipse.com/2012/12/06/processor-expert-maxim-i2c-rtc-driver-the-arduino-data-logger-shi...

Erich

1,688件の閲覧回数
mjbcswitzerland
Specialist V

Hi

See chapter 3 of

http://www.utasker.com/docs/uTasker/uTaskerIIC.PDF

The DS1307 is supported on the KL46 in the uTasker project: http://www.utasker.com/forum/index.php?topic=1721.0

Regards

Mark

http://www.utasker.com/kinetis.html