Interfacing DS1307 with KL46

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing DS1307 with KL46

1,877 Views
abulhasan_cas
Contributor I

Hi all,

     Good day to you.

     I'm using KL46 processor and we are in need to interface an external RTC chip DS1307 with KL46. Can anyone suggest me how to get the output of DS1307 and feed it to the KL46 in I2C.

Abul Hasan

0 Kudos
Reply
2 Replies

1,668 Views
BlackNight
NXP Employee
NXP Employee

I have created an open source Processor Expert component which supports both the DS3232 and DS1307:

http://mcuoneclipse.com/2012/12/06/processor-expert-maxim-i2c-rtc-driver-the-arduino-data-logger-shi...

Erich

1,668 Views
mjbcswitzerland
Specialist V

Hi

See chapter 3 of

http://www.utasker.com/docs/uTasker/uTaskerIIC.PDF

The DS1307 is supported on the KL46 in the uTasker project: http://www.utasker.com/forum/index.php?topic=1721.0

Regards

Mark

http://www.utasker.com/kinetis.html