I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds. Can anyone suggest me the feasibility for the same in KL46 controller ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds. Can anyone suggest me the feasibility for the same in KL46 controller ?

1,591件の閲覧回数
yusupkhan
Contributor II

I'm using lptmr delay in KL46 controller. I was able to provide the minimum delay in 1millisecond for instruction. I require the delay in microsecond or possibly in nanoseconds.  Can anyone suggest me the feasibility for the same in KL46 controller ?

ラベル(1)
0 件の賞賛
返信
1 返信

1,394件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You can select the source of the LPTMR clock.

If you have an 8MHz oscillator connected and use this as source you will have 125ns timer resolution.

regards

Mark

0 件の賞賛
返信