Info on K70

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Info on K70

1,214件の閲覧回数
sudeepaithal
Contributor I

Hello,

Can anyone please tell me what is the maximum size of external flash that can be connected to K70 and also the source from where this info was taken

Thanks

Sudeep

ラベル(2)
0 件の賞賛
返信
1 返信

1,168件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Sudeep,

as you can see in the Reference Manual you have the option to use Multiplexed 32-bit address and 32-bit data. Therefore you can address 2^32 bytes.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信