Info on K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Info on K70

1,278 Views
sudeepaithal
Contributor I

Hello,

Can anyone please tell me what is the maximum size of external flash that can be connected to K70 and also the source from where this info was taken

Thanks

Sudeep

0 Kudos
Reply
1 Reply

1,232 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Sudeep,

as you can see in the Reference Manual you have the option to use Multiplexed 32-bit address and 32-bit data. Therefore you can address 2^32 bytes.


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply