If I change the ADC settings, do I need to ADC calibrate again?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

If I change the ADC settings, do I need to ADC calibrate again?

ソリューションへジャンプ
1,744件の閲覧回数
rs__zen
Contributor I

Hi.

I'm using the MKE14F MCU.

In ref manual, it written It is mandatory to calibrate the ADC after power up or reset.

So, after calibrating once, for example, if I change the conversion mode from 8-bit to 12-bit, do I need to calibrate again?

Or is such a change in settings irrelevant to calibration?

Please tell me.

Thank you.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,738件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi rhata,

You don't need to calibrate again after change the conversion mode from 8-bit to 12-bit.

AN5314 ADC Calibration on Kinetis E+Microcontrollers may help you better understand.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,729件の閲覧回数
rs__zen
Contributor I

Hi Robin.

Thank you for your answer !!

Best regards.

0 件の賞賛
返信
1,739件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi rhata,

You don't need to calibrate again after change the conversion mode from 8-bit to 12-bit.

AN5314 ADC Calibration on Kinetis E+Microcontrollers may help you better understand.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信