I want to use FIRC clock source to config FlexCAN module ,But it failed. So I want to check Whether support FIRC clock source as CAN Protocol Interface (CPI) clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I want to use FIRC clock source to config FlexCAN module ,But it failed. So I want to check Whether support FIRC clock source as CAN Protocol Interface (CPI) clock

960 Views
superboss
Contributor I

I want to use FIRC clock source to config FlexCAN module ,But it failed. So I want to check Whether support FIRC clock source as CAN Protocol Interface (CPI) clock

0 Kudos
Reply
1 Reply

849 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

There is a note in the datasheet(KE1xFP100M168SF0) of Kinetis KE1xF.

Fast internal RC Oscillator is compliant with CAN and LIN standards.

FIRC CAN.jpg

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply