How to set up the Sniffer?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set up the Sniffer?

1,109 Views
aroplane
Contributor III

Hi,

I am experiencing a problem when testing the USB on the board TWR-K64. I successfully downloaded the demo project "usb_examples-usb_device_hid_generic - bm" into the board, and the USB device got enumerated. A PC software is needed to verify the firmware. I found there is a readme.pdf in the project showing how to edit the c# code for the display. I did so. However, the software always displays as below when it is running (also attached). It is not that picture shown in readme.pdf. I couldn't find where to input Device Vendor Id and Device Product ID. The PC OS is 64-bit Windows 7. I already selected x86 CPU platform in the project. 

Could you please tell me what the possible reasons could be? Thank you very much.

pastedImage_1.png

Best regards,
Lei Peng
Labels (2)
0 Kudos
Reply
0 Replies