How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

Jump to solution
4,939 Views
anand-k
Contributor III

How to load code(elf binary code) into KL25 and make it run out of reset w/o debugger connection?..openSDA or USB multilink will be used just to download code into controller.

Labels (1)
0 Kudos
Reply
1 Solution
3,778 Views
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

View solution in original post

0 Kudos
Reply
1 Reply
3,779 Views
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

0 Kudos
Reply