How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

ソリューションへジャンプ
5,042件の閲覧回数
anand-k
Contributor III

How to load code(elf binary code) into KL25 and make it run out of reset w/o debugger connection?..openSDA or USB multilink will be used just to download code into controller.

ラベル(1)
0 件の賞賛
返信
1 解決策
3,881件の閲覧回数
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,882件の閲覧回数
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

0 件の賞賛
返信