How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to load code(binary code) into KL25 and make it run out of reset w/o debugger connection?

跳至解决方案
3,960 次查看
anand-k
Contributor III

How to load code(elf binary code) into KL25 and make it run out of reset w/o debugger connection?..openSDA or USB multilink will be used just to download code into controller.

标签 (1)
0 项奖励
回复
1 解答
2,800 次查看
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,801 次查看
rgd04c
NXP Employee
NXP Employee

Hi Anand,

Not sure if I understand correctly but have you used the OpenSDA Bootloader mode?. You can just drag and drop a binary once the KL25 is recognized as a Mass storege device in the computer, just like a thumb drive!

Please refer to page 6 of attached document.

regards,

Gonzalo

0 项奖励
回复