How to get clock config tool working with KV56

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get clock config tool working with KV56

ソリューションへジャンプ
3,083件の閲覧回数
derekcook
Senior Contributor I

Hello, 

I have a KV56 project and I'm trying to get the clock tool running with it to generate the clock_config files but when I click on MCUXpresso Config Tools I get this message: 

derekcook_0-1656526608143.pngderekcook_0-1656526608143.png

 

I took the clock_config files from the sdk examples and modified my oscillator frequency to me external oscillator of 12MHz. 

derekcook_1-1656526672138.pngderekcook_1-1656526672138.png

 

This does allow the debug console to work, but I'm afraid I missed something.  I also set board XTAL_FREQ to 12MHz

derekcook_2-1656526743409.pngderekcook_2-1656526743409.png

 

However, when I check CLOCK_GetCoreSysClkFreq it is not close to 240MHz for the HS clock. 

derekcook_4-1656526835238.pngderekcook_4-1656526835238.png

 

derekcook_3-1656526817496.pngderekcook_3-1656526817496.png

 

 

 

 

 

0 件の賞賛
返信
1 解決策
3,080件の閲覧回数
derekcook
Senior Contributor I

I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code

derekcook_0-1656528965962.pngderekcook_0-1656528965962.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,029件の閲覧回数
derekcook
Senior Contributor I

Nope! I figured it out! 

0 件の賞賛
返信
3,081件の閲覧回数
derekcook
Senior Contributor I

I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code

derekcook_0-1656528965962.pngderekcook_0-1656528965962.png

 

0 件の賞賛
返信
3,055件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

I see you already figured it out, do you have another question about it?

0 件の賞賛
返信