How to get clock config tool working with KV56

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to get clock config tool working with KV56

Jump to solution
2,291 Views
derekcook
Senior Contributor I

Hello, 

I have a KV56 project and I'm trying to get the clock tool running with it to generate the clock_config files but when I click on MCUXpresso Config Tools I get this message: 

derekcook_0-1656526608143.png

 

I took the clock_config files from the sdk examples and modified my oscillator frequency to me external oscillator of 12MHz. 

derekcook_1-1656526672138.png

 

This does allow the debug console to work, but I'm afraid I missed something.  I also set board XTAL_FREQ to 12MHz

derekcook_2-1656526743409.png

 

However, when I check CLOCK_GetCoreSysClkFreq it is not close to 240MHz for the HS clock. 

derekcook_4-1656526835238.png

 

derekcook_3-1656526817496.png

 

 

 

 

 

0 Kudos
Reply
1 Solution
2,288 Views
derekcook
Senior Contributor I

I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code

derekcook_0-1656528965962.png

 

View solution in original post

0 Kudos
Reply
3 Replies
2,237 Views
derekcook
Senior Contributor I

Nope! I figured it out! 

0 Kudos
Reply
2,289 Views
derekcook
Senior Contributor I

I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code

derekcook_0-1656528965962.png

 

0 Kudos
Reply
2,263 Views
_Leo_
NXP TechSupport
NXP TechSupport

I see you already figured it out, do you have another question about it?

0 Kudos
Reply