How to disable reset pin output from MK24FN1M0VLQ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to disable reset pin output from MK24FN1M0VLQ12

Jump to solution
2,055 Views
yuanli
NXP Employee
NXP Employee

Hi,

Customer found recently that the RESET# pin from MK24 can have output when the chip is being reset by internal watchdog.

Can this output be disabled? Please help advise, thanks.


Best regards,

Ryan

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,756 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,757 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,756 Views
yuanli
NXP Employee
NXP Employee

Hi Jorge,

Thanks for your confirmation.

Best regards,

Ryan

0 Kudos
Reply