How to disable reset pin output from MK24FN1M0VLQ12

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to disable reset pin output from MK24FN1M0VLQ12

ソリューションへジャンプ
2,696件の閲覧回数
yuanli
NXP Employee
NXP Employee

Hi,

Customer found recently that the RESET# pin from MK24 can have output when the chip is being reset by internal watchdog.

Can this output be disabled? Please help advise, thanks.


Best regards,

Ryan

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,397件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,398件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,397件の閲覧回数
yuanli
NXP Employee
NXP Employee

Hi Jorge,

Thanks for your confirmation.

Best regards,

Ryan

0 件の賞賛
返信