How to disable reset pin output from MK24FN1M0VLQ12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to disable reset pin output from MK24FN1M0VLQ12

跳至解决方案
2,039 次查看
yuanli
NXP Employee
NXP Employee

Hi,

Customer found recently that the RESET# pin from MK24 can have output when the chip is being reset by internal watchdog.

Can this output be disabled? Please help advise, thanks.


Best regards,

Ryan

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,740 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,741 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Yuan Li:

Unfortunately in Kinetis K parts such as K24 it is not possible to isolate the reset pin from the internal reset caused by the watchdog.

For Kinetis L MCUs, there is a bit in the flash configuration space that allows disabling the Reset_b pin (search for FTFA_FOPT[RESET_PIN_CFG])


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,740 次查看
yuanli
NXP Employee
NXP Employee

Hi Jorge,

Thanks for your confirmation.

Best regards,

Ryan

0 项奖励
回复