How to determine/confirm Cortex-M CPU speed using Serial Wire Viewer !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to determine/confirm Cortex-M CPU speed using Serial Wire Viewer !

1,884件の閲覧回数
robertboys
Contributor IV

Hello

I devised an easy way to determine the CPU speed using ARM Serial Wire Viewer.

This works with any Kinetis or LPC Cortex-M3, M4 or M7.  Assume also Cortex-M23 or 33.  No Cortex-M0 (has no SWV)

I posted it here:  Application Note 297: Using Serial Wire Viewer to Confirm CPU Speed 

This uses eval version of Keil MDK and any ULINK or a Segger J-Link.

Tanks

Bob  Boys

ARM

1 返信

1,531件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Bob,

Thank you for your input :smileywink:

Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信