How read ADC pin (NOT procesor expert)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How read ADC pin (NOT procesor expert)

1,945件の閲覧回数
sergheiplamadea
Contributor I

I elementary instruction to read value from ADC-pin

thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,754件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Please download Kinetis 100MHz example code from below link, which provides ADC application demo code (not based on Processor Expert):

KINETIS512_V2_SC (Kinetis 100MHz Rev 2 Example Projects)

TWR-K60D100M: Kinetis K60 100 MHz MCU Tower System Module


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,754件の閲覧回数
yvesb
Contributor II

Hi Serghei,

you can check my example here https://community.freescale.com/thread/321127

and read the appropriate manual for your microcontroller. especially if you are not a processor expert :smileywink:

regards,

Yves

0 件の賞賛
返信