How read ADC pin (NOT procesor expert)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How read ADC pin (NOT procesor expert)

1,916 Views
sergheiplamadea
Contributor I

I elementary instruction to read value from ADC-pin

thanks

Labels (1)
0 Kudos
Reply
2 Replies

1,725 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Please download Kinetis 100MHz example code from below link, which provides ADC application demo code (not based on Processor Expert):

KINETIS512_V2_SC (Kinetis 100MHz Rev 2 Example Projects)

TWR-K60D100M: Kinetis K60 100 MHz MCU Tower System Module


Wish it helps.

Best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,725 Views
yvesb
Contributor II

Hi Serghei,

you can check my example here https://community.freescale.com/thread/321127

and read the appropriate manual for your microcontroller. especially if you are not a processor expert :smileywink:

regards,

Yves

0 Kudos
Reply