How do I selsct a MCU with just an .axf file to write

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I selsct a MCU with just an .axf file to write

1,016 Views
erik_hedberg
Contributor I

how do I select an MCU with just an .axf file to write

0 Kudos
Reply
1 Reply

990 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Erik,

Hope you are doing well.

Could you please share what microcontroller you are using so I can provide detail instructions if needed. 

If you are working with MCUXpresso IDE, you may download the SDK of the microcontroller you are using on the MCUXpresso Website

Once downloaded, you may import the SDK to MCUXpresso IDE, then you can import an example. 

When you build the project, the axf file is created automatically.

pastedImage_2.png

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply