How do I capture one image with K82F & OV7670 camera?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How do I capture one image with K82F & OV7670 camera?

6,848 次查看
jwhammel1
Contributor I

We have the example running that allows the K82F and the OV7670 camera to send video to Skype.  We are trying to just capture one picture from the live video and save it in the easiest place. We are having trouble locating the files that send the video to Skype.  We were thinking that this would be the best place to add code to save a single frame.

标签 (1)
标记 (2)
0 项奖励
回复
11 回复数

6,535 次查看
jwhammel1
Contributor I

I looked at that post before and even replied to it days ago but no reply back. I couldn't find the mentioned app note:  (Refer app note: Relocating Code and Data Using the KDS GCC Linker File (.ld) for Kinetis).

0 项奖励
回复

6,535 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

6,535 次查看
jwhammel1
Contributor I

I'm sorry, I didn't see the attachments,  that's fixed now.  After adding the file we are left with these errors?

0 项奖励
回复

6,535 次查看
jingpan
NXP TechSupport
NXP TechSupport

Yes, please try other browser.

0 项奖励
回复

6,535 次查看
jwhammel1
Contributor I

What about the errors.
'u16CameraFrameBuffer' undeclared here (not in a function) main.c /app_demo_k80_flexio_camera_MK80FN256VDC15/sources line 99 C/C++ Problem

0 项奖励
回复

6,535 次查看
jingpan
NXP TechSupport
NXP TechSupport

Please add

  static uint16_t  __attribute__((section (".myBufSection"))) u16CameraFrameBuffer[OV7670_FRAME_PIXELS] ;

This problem is mentioned in the link https://community.nxp.com/thread/455608 

0 项奖励
回复

6,535 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

There is a anpplication note AN5275 which talk about useing FlexIO for parallel camera interface. It use K80 and ov7670 as example. It has software demo. You can refer to it.

Regards,

Jing

0 项奖励
回复

6,535 次查看
jwhammel1
Contributor I

We initially had 6 errors but corrected 2 of them by including the missing files manually by following the instructions on webpage: AN5275_SW FlexIO demo compilation error in KDS  shown below.  We are trying to figure out the step in main.c but the application note "Relocating Code and Data Using the KDS GCC Linker File (.ld) for Kinetis" is not there. Do you have any recommendations for the remaining errors?

0 项奖励
回复

6,535 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Attachment is the link file. You should change the project link file at here

pastedImage_1.png

Regards,

Jing

0 项奖励
回复

6,531 次查看
jwhammel1
Contributor I

Hello,

Thanks for the response, I am referring to the application note and the

AN5275_SW.zip (attached zip file) found on the nxp website. I am unable to

find the .ld file mentioned by you in the kds directory, however other

launches file are do available.

For reference i have attached the zip file and the image. Thanks for the

future response.

0 项奖励
回复

6,531 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Can't you see the attachment I pasted in my reply? Maybe you should change a browser. AN5275sw hasn't ld file. It use KDS's default ld file but need to be modify.

Regards,

Jing

0 项奖励
回复