Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

1,244件の閲覧回数
williamf
Contributor I

Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

0 件の賞賛
返信
1 返信

1,106件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I am afraid that the NXP USBDCD only compliant with the industry standard specification: USB Battery Charging

Specification, Revision 1.1.

0 件の賞賛
返信