Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

1,251 Views
williamf
Contributor I

Hi, Is K21 USB device charger detection (USBDCD) fully compliant with USB battery charger spec 1.2? Can it detect 3rd party chargers like APPLE? Thanks.

0 Kudos
Reply
1 Reply

1,113 Views
miduo
NXP Employee
NXP Employee

Hi,

I am afraid that the NXP USBDCD only compliant with the industry standard specification: USB Battery Charging

Specification, Revision 1.1.

0 Kudos
Reply