Has anyone tried using DMA with FlexIO?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Has anyone tried using DMA with FlexIO?

2,003件の閲覧回数
Xlerb
Contributor II

Using FlexIO as SPI on KL17 and would like to use a DMA controller to feed it.

Ref manual says it's possible. Anyone tried it?

Are there any examples?

Thanks,

Martin.

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,793件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Martin,
You can build and download the SDK_2.1_MKL17Z256xxx4 from MCUXpresso Config Tools.
There are two examples seems meet your needs.

flexio spi dma.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,793件の閲覧回数
Xlerb
Contributor II

Hi Robin,

Thanks that was helpful.

It's a shame that the documentation in the reference manual isn't good enough to write code without needing to spend a lot of time looking at examples.

Anyway, thanks for your help.

Regards,

Martin.

0 件の賞賛
返信