Has anyone tried using DMA with FlexIO?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone tried using DMA with FlexIO?

1,979 Views
Xlerb
Contributor II

Using FlexIO as SPI on KL17 and would like to use a DMA controller to feed it.

Ref manual says it's possible. Anyone tried it?

Are there any examples?

Thanks,

Martin.

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,769 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Martin,
You can build and download the SDK_2.1_MKL17Z256xxx4 from MCUXpresso Config Tools.
There are two examples seems meet your needs.

flexio spi dma.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

1,769 Views
Xlerb
Contributor II

Hi Robin,

Thanks that was helpful.

It's a shame that the documentation in the reference manual isn't good enough to write code without needing to spend a lot of time looking at examples.

Anyway, thanks for your help.

Regards,

Martin.

0 Kudos
Reply